DIN#.STATE
Description
Reads the state of one digital input according to the number identified in the command.
Examples
Code
--> DIN1.STATE 1
Context
For more information see Digital I/O.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read Only |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | N/A |
| Data Type | Integer |
| See Also | |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
|
Copyright © 2018 Kollmorgen |
|